Tripp Lite

Testimonial

Site Map
Model Number Search
     
  Tripp Lite’s APS Inverters Give EngenderHealth the Power to Improve Women’s Health Worldwide

Tripp Lite, a world leader in the manufacture of power protection equipment, is proud to announce its high quality line of APS (Alternative Power Sources) Inverters/Battery Chargers is being praised by EngenderHealth for providing them with consistent power for critical network servers through daily blackouts and brownouts. Tripp Lite’s APS Inverters have proven to be a tremendous success for EngenderHealth, a worldwide healthcare institution that provides medical expertise, training and technical assistance to countries where basic women’s healthcare needs are urgent.

“We are definitely satisfied Tripp Lite customers as our new inverter system has effectively delivered us from the frustrations of almost daily losses of computer work caused by the power outages which are so common in Kenya,” states Dr. Albert E. Henn, M.D. EngenderHealth’s AMKENI Project Director in Nairobi, Kenya. “It has been a miracle. The power still goes off, but our network server now stays on and we keep right on working.”

EngenderHealth works with public and private health providers to improve the quality of healthcare women receive in countries throughout the world. Their main contribution is in the publication of training materials for health workers in both print and online formats in clinical technique appropriate for low resource settings. EngenderHealth is partners with several, key, global policy-setting agencies, such as the World Health Organization, the United Nations Population Fund and the U.S. Centers for Disease Control and Prevention.

A complete Tripp Lite APS Inverter System has become an essential tool in assuring quality healthcare for EngenderHealth. Dr. Henn states, “Because our work is highly computer-dependent, we can’t afford to lose work and miss deadlines. Power outages are frequent in Kenya and without reliable current we lose valuable data and contracting opportunities.”

“This is the kind of success story we love to hear and a key reason we are in the power protection business,” states Vipin Sharma, Tripp Lite Regional Director of the Middle East and Africa. “Our new 230V APS Inverter line was specifically designed for sporadic power problems such as this, and it’s great to know this technology is being put to good use in practical applications.”

Tripp Lite’s new line of 230V APS PowerVerter® DC-to-AC Inverters/Battery Chargers feature the latest generation components and provide users with the most reliable and safe Alternative Power Sources for large loads and critical equipment.

Multi-function APS PowerVerters offer auto line-to-battery transfer and an integrated charging system to serve as an extended run UPS, a standalone power source, or an automotive inverter. These PowerVerters provide AC power to your equipment while utility power is available and charge an array of user-supplied DC batteries at the same time. When AC power is not available, such as during blackouts or when a vehicle equipped with an APS PowerVerter is on the road, APS PowerVerters quickly and automatically switch to providing connected equipment with frequency controlled AC power drawn from attached batteries. Sophisticated electronic circuitry provides high peak surge power (up to 200% of rated output) to start and run heavy draw devices. Automatic overload protection protects the system from damage if overloaded. High-efficiency output is frequency controlled to support sensitive loads such as computers.

 

MEDIA INFORMATION
Contact: pr@tripplite.com

 

     
     
     
 
© 2008 Tripp Lite. All Rights Reserved.