| |
|
 |
 |
 |
 |
| |
|
|
|
| |
Q: |
How does an on-line UPS differ from a line-interactive
or standby UPS? |
|
| |
A: |
A line-interactive or standby UPS passes utility
power to connected equipment, filtering out surges, spikes, and
line noise as it does so. When a severe brownout or a power outage
occurs, the DC to AC inverter will switch on, supplying a modified
sine wave output from battery. An on-line UPS uses a double conversion
process: incoming AC is converted to DC, and DC is converted back
to AC. Since the DC-to-AC inverter runs constantly there is no switching
time, and connected equipment receives pure, filtered sine wave
output at all times. |
|
| |
|
|
|
| |
Q: |
What is the difference between SMART and OMNISMART UPS
Systems? |
|
| |
A: |
SMART UPS Systems have an enhanced microprocessor that can monitor
and report more UPS variables (e.g. UPS input voltage, load, and
battery capacity). OMNISMART UPS Systems can report three UPS variables
only: UPS in line mode, on battery, and battery low. |
|
| |
|
|
|
| |
Q: |
What are the largest VA-rated UPS Systems manufactured
by Tripp Lite that run on 120VAC input and output 120VAC?
|
|
| |
A: |
- SU3000RTXL3U
- SU30000XL
- SMART3000RM2U
- SMART3000VS
- SMART3000NET
To utilize full UPS output potential, a connection to a dedicated
30-amp circuit is necessary. For more information, see individual
UPS specifications.
|
|
| |
|
|
|

| |
|
|
|
| |
Q: |
Can a UPS be plugged into one another UPS (daisy chained)? |
|
| |
A: |
No, UPS systems cannot be daisy chained. If you require additional capacity or battery runtime, select a larger UPS or one that accepts external battery packs. If connected equipment has redundant power supplies and redundancy is required, it is recommended that two UPS systems, plugged into two different circuits, be used. |
|
| |
|
|
|
| |
Q: |
Can the UPS alarm be permanently disabled? |
|
| |
A: |
No, the UPS alarm cannot be permanently disabled, but select Tripp Lite UPS models permit the alarm to be muted when the UPS is operating in battery mode. |
|
| |
|
|
|
| |
Q: |
Why won't the "Load Active Meter" illuminate when my UPS is connected to a load of less than 25%?
|
|
| |
A: |
The "Load Active Meter" will not illuminate to show a load percentage LED until the UPS output load exceeds 25%. |
|
| |
|
|
|

| |
|
|
|
| |
Q: |
Why won't my new UPS power up? |
|
| |
A: |
Tripp Lite UPS systems must be charged for 4-6 hours
to bring the battery up to 90% capacity. Under certain conditions
no LEDs will illuminate until the battery is charged. |
|
| |
|
|
|
| |
Q: |
My on-line UPS shows only two LEDs (Line and Load), and
does not pass AC power to the output receptacles. |
|
| |
A: |
Press and hold the ON button and release it as soon as you hear
a beep. Three LEDs will illuminate (Line, Load, and Online), and
power will be passed to the output receptacles. |
|
| |
|
|
|
| |
Q: |
My INTERNET350/525/550/750 UPS constantly beeps and shows
a red LED. |
|
| |
A: |
Turn off all equipment connected to the UPS, unplug the AC cord
from the wall outlet, then press and hold the OFF button until the
unit is completely turned off (about 4 seconds). Wait for an additional
10 seconds to make sure that there are no LEDs flashing. Once the
unit has been completely turned off, plug the AC cord back into
the wall outlet. When reconnected to AC power, the unit will beep
several times. It will beep several more times after performing
a self-test. The line LED will then illuminate to indicate that
the UPS has re-initialized. |
|
| |
|
|
|
| |
Q: |
My Tripp Lite UPS isn't working. Is there a service center
in my area where the unit can be repaired? |
|
| |
A: |
If your UPS is under warranty, Tripp Lite will replace it or provide
other options. Contact Tripp Lite Technical Support at 773-869-1234
or email us for assistance. |
|
| |
|
|
|

| |
|
|
|
| |
Q: |
I have an older UPS system. How can I get
information about battery replacement? |
|
| |
A: |
Contact Tripp Lite Technical Support at 773-869-1234
or by email. Have
the UPS serial number, stock number, and date code available at
the time of your call. A technician will identify the correct replacement
battery for your UPS. You can also use our online R.B.C.
Selector Guide to identify the correct replacement battery for
your system. |
|
| |
|
|
|
| |
Q: |
My UPS has been in storage and now it will not turn on.
What's wrong? |
|
| |
A: |
When you store a UPS for an extended period, it must be plugged
in and allowed to charge for 24 hours once every 3 to 6 months.
Unless this is done, the UPS batteries will discharge to an unrecoverable
point and the UPS will require new batteries. |
|
| |
|
|
|
| |
Q: |
How much additional runtime do external battery packs
provide for my UPS? |
|
| |
A: |
There is no specific amount of additional runtime that a given
battery pack will provide for a given UPS; this depends on the demands
of the connected load. For assistance in determining an estimated
runtime, call Tripp Lite Technical Support, 773-869-1234, with your
power draw information, UPS model, and battery pack model. Our interactive
UPS System Selector
Guide may also be used to estimate runtimes. |
|
| |
|
|
|
| |
Q: |
Where can I send my old UPS batteries for recycling? |
|
| |
A: |
For battery recycling within the United States:
Call 1-800-SAV-LEAD or 1-800-8-BATTERY (1-800-822-8837), or visit
the Rechargeable Battery
Recycling Corporation for information about recycling in your
area.
Call 1-800-677-8278 or visit BatteriesPlus.com
to access Batteries Plus retail locations nationwide that provide
battery recycling.
Ship batteries (freight prepaid) to: Tripp Lite, 1111 W. 35th St. Chicago IL 60609, Attn: USED BATTERIES.
|
|
| |
|
|
|



|