Tripp Lite

Frequently Asked Questions

Tripp Lite Solutions - Line Conditioners & Isolation Transformers

Site Map
Model Number Search


Other Resources

Power Protection Glossary
Pre-Sales Inquiries
Technical Support
Product Selectors
UPS Selection Worksheets (PDF)
Where to Buy
Contact Tripp Lite

 
Line Conditioners & Isolation Transformers
UPS Systems | Surge Suppressors | Line Conditioners & Isolation Transformers
Inverters & Inverter/Chargers | KVM Switches | Cables & Connectivity
       
  Q:

Can your line conditioner be used with generators?

 
  A:

Yes. But while Tripp Lite line conditioners will stabilize voltage, filter high frequency noise, and protect against surges and spikes, they will not correct frequency or clean up a distorted waveform produced by a generator.

 
       
  Q:

Can you plug a line conditioner into an inverter?

 
  A:

No. Inverters do not require a line conditioner as they already put out clean AC power. In addition, most inverters put out a modified sine wave. Line conditioners require true sine wave power as the surge suppression inside senses the changed waveform as a surge and will shunt it back to the inverter, thus damaging the inverter.

 
       
  Q:

Can a line conditioner change 120V to 240V or vice versa?

 
  A:

No.

 
       
  Q:

What is the difference between a line conditioner and an isolation transformer?

 
  A:

That depends on whom you ask. Different manufacturers have different definitions of what constitutes a line conditioner. To some an isolation transformer is a line conditioner. Tripp Lite line conditioners will stabilize voltage, filter high-frequency noise, and protect against surges and spikes, but they do not provide line isolation. Tripp Lite isolation transformers provide line isolation but do not correct for voltage variations.

 
       
  Q:

I had a 2-second power outage and your line conditioner did not keep my equipment running. Why?

 
  A:

It is not designed to back up equipment during a power outage, as it does not have an internal battery.

 
       
  Q:

I hear clicking noise coming out of my line conditioner. Is this normal?

 
  A:

Yes. The clicking noise you hear are the relays (taps) adjusting the incoming AC voltage.

 
       
  Q:

My UPS does not have line conditioning. Can I use a line conditioner with my UPS?

 
  A:

Tripp Lite does not recommend it. If the line conditioner is used on the input side of the UPS, the switching taps may cause the UPS to run from battery power for a few seconds. If this happens often enough the battery in the UPS will discharge faster than it recharges. If the line conditioner is used on the output side of the UPS, it may recognize the PWM output from the inverter as a surge and become a direct short to the UPS.

 
       
  Q:

Will your line conditioner correct frequency?

 
  A:

No.

 
       
  Q:

Will your line conditioner change a square wave or PWM wave into a sine wave?

 
  A:

No. The LS/LC/LCR series will do nothing to change the shape of the waveform fed to them.

 
       


Line Conditioners Solve:


Isolation Transformers Solve:


 
Couldn't find the answer to your question here?
Email Tripp Lite Technical Support


© 2008 Tripp Lite. All Rights Reserved.