There are many rating systems that measure surge protection:
Joule Ratings - Joule ratings measure a surge suppressor's ability
to absorb surges. Joules are a way of measuring energy. In general,
200 joules will give you basic protection, 400 joules provide good
protection and anything with over 600 joules can be considered exceptional.
Tripp Lite surge suppressors boast ratings of up to 5700 joules
and have the advanced circuitry to back them up!
Surge Amp Ratings - higher ratings offer more protection. Although
often replaced by Joule ratings, Amp levels are another important
factor in determining surge strength. Once again, you should go
for the highest amp protection levels you can find.
UL 1449 Voltage Let-through Ratings - 500, 400 & 330. Underwriter
Laboratories tests each surge suppressor and rates them according
to the amount of voltage they "let-through" to your equipment. The
lower the let-through voltage, the better the surge suppressor is.
UL established the 330 volt let-through as the benchmark because
lower ratings added no real benefit to equipment protection, while
surge components, forced to work harder, failed prematurely. |