Tripp Lite

Power Management Tools

SOFTWARE / PowerAlert

Site Map
Model Number Search
     
 

PowerAlert FAQ
Frequently Asked Questions

Find answers to the most commonly asked questions about PowerAlert Management Software. Click on a question below to jump to its answer, or scroll down to browse through all of this valuable information. If you need additional information please call our technical support department at (773) 869-1234.

 

 

Question:
I am going to use Windows 2000 Power Management instead of PowerAlert. Do I need any Tripp Lite software?

Answer:
You should download and install Power Management for Windows 2000. This file contains drivers for Tripp Lite UPS systems. Do not download or install this file if you are going to use PowerAlert.

 

 

Question:
Which should I do first, connect my UPS to my computer with a communication cable or install PowerAlert?

Answer:
Connect your computer to your UPS with a communication cable before installing PowerAlert.

 

 

Question:
I lost the cable that came with my UPS. Can I use a different cable?

Answer:
UPS systems with DB9 connectors require a special cable for RS-232 communications that is available from Tripp Lite.

Any USB cable can be used to connect an USB-capable UPS to a computer.

 

 

Question:
Is PowerAlert compatible with Windows XP?

Answer:
Yes.

 

 

Question:
If PowerAlert shuts my computer down during a blackout, will it turn the computer back on when power is restored?

Answer:
No. Your computer’s BIOS setup determines if it starts when power is restored.

 

 

Question:
When I start PowerAlert, I see a half-full battery icon in my system tray and then my system shuts down. What action should I take?

Answer:
You may experience this problem if you chose a contact closure UPS (BC Pro, OmniPro, OmniSmart and Internet Office models are all contact closure UPSs) and started PowerAlert without properly connecting the communications cable. Make sure that you have chosen the correct UPS model and connected the proper communications cable from the UPS to the communications port you chose during setup.

 

 

Question:
How do I perform a remote shutdown?

Answer:
You can configure a remote system to be shut down by using the PowerAlert Remote Shutdown Server.

  1. Start the PowerAlert Server on the computer connected to the UPS.

  2. On the remote system, use the PowerAlert Server Setup application to configure the remote system as a Remote Shutdown Server.

  3. You will need to know the IP address of the computer running the PowerAlert Server (or you can use the built-in autodiscover feature to find computers that are running the PowerAlert Server).

  4. When the power fails, the PowerAlert Server will send a message to the Remote Shutdown Client. You can configure a shutdown delay (time from receipt of an "on battery" message until the computer shuts down).

 

 

Question:
How do I use communication ports 3 and 4 when running PowerAlert?

Answer:
If COM3 or COM4 are properly configured, simply choose COM3 or COM4 from PowerAlert Server Setup and then start the PowerAlert Server. Other communications ports, although not shown in the list, can also be used by editing the text file /PowerAlert/INI/Server.ini. Change the line "Port=xxx" to "Port=COM5", for example. If you change the selected communications port while PowerAlert Server is running, you will be prompted to restart the server.

 

 

Question:
How can I configure PowerAlert shutdown times?

Answer:
Use the Event Manager in the PowerAlert Client.

  1. From the PowerAlert Client, select menu option Events/Event Manager.

  2. From the drop-down list, select the UPS event that you wish to modify.

  3. Click the Shutdown tab. The shutdown delay times will be displayed for both Operating System shutdown and UPS shutdown.

  4. Change the shutdown delays to fit your operating environment.

NOTE: You should select a UPS shutdown time that is longer than the operating system shutdown time. Make sure that you provide enough time for the operating system to completely shut down before the UPS shuts down.

 

 

Question:
What does PowerAlert do with open files when it shuts down the operating system?

Answer:
PowerAlert saves open files on all Windows platforms (95, 98, NT, 2000). All open documents will be saved in the DataSafe sub-directory. All files will have a file name with the format TL_####.ext, where #### is a number assigned by PowerAlert and ext. is the extension of the associated application (.doc for Word documents, for example). The documents that get saved in the DataSafe directory are copies of the original documents.

 

 

Question:
Will PowerAlert work in my mixed-platform environment consisting of NetWare, Windows and UNIX computers?

Answer:
PowerAlert uses TCP/IP to allow communication across multiple platforms including NetWare, Windows and UNIX operating systems. To monitor the UPS on another computer, perform the following steps:

  1. From the PowerAlert Client System menu, add the IP address or host name of the computer you wish to monitor. This will be stored in the system list.

  2. From the PowerAlert Client View menu, choose the computer you wish to monitor from the system list.

 

Question:
When using a UPS that has multiple communication ports, which cables should I use?

Answer:
The 73-0743 cable should be connected to the port that is labeled Smart/LAN 4.x (example: Smart/LAN 4.1). This port and cable combination is used for smart communication. The other ports will be labeled Basic/LAN 2.x (example: Basic/LAN 2.1). These ports should use the 73-0844 cable for monitoring.

If only the smart port (Smart/LAN 4.x) is to be used for monitoring, the Basic/LAN 2.x ports should be disabled using the dip switches on the back of the UPS.

 

 

Question:
When I have a power failure, PowerAlert shuts down my operating system but not my UPS. Why?

Answer:
If your UPS is a contact closure UPS (BC Pro, OmniPro, OmniSmart, and Internet Office models are all contact closure UPSs), your UPS will shut off at the time specified in Event Manager after a power failure event only if you are using PowerAlert on the Windows NT platform.

NOTE: Your contact closure UPS will always shut off two minutes after the UPS reaches the low battery condition, regardless of your operating system.

 

 

Question:
How can I quickly review my power outage history?

Answer:
From PowerAlert Client, select the Event Log option from the View menu. You can filter by date by entering the desired date range at the bottom of the Event Log screen.

 

 

Question:
Can I have more than one computer communicating with the same UPS?

Answer:
Under normal circumstances, we recommend using the Remote Shutdown Client for this type of scenario. However, Tripp Lite now offers a "Y" cable that allows up to two computers to perform smart communication with a single UPS.

 

 

Question:
Does PowerAlert have the capability to limit broadcast messages to certain users?

Answer: PowerAlert broadcast messages get sent to the computer's entire workgroup or domain. If a user prefers to only have select users notified, these users can be notified via PowerAlert's email feature.

 

 

Question:
How do I know whether to choose Home/Office or Network/Office when installing PowerAlert on a Windows machine?

Answer:
The user should always choose Network Mode unless the computer does not have the TCP/IP protocol installed.

To see if TCP/IP is installed:

  1. Select Network from the system Control Panel.

  2. Choose the configuration tab.

  3. If the TCP/IP protocol is listed with the words "dial up adapter" next to it, the computer only has TCP/IP for dial-up networking.

PowerAlert requires the TCP/IP protocol to be bound to a network interface card and have a specific IP address assigned to the computer in order to run PowerAlert in network mode.

 

 

Question:
What is "load shedding"?

Answer:
"Load shedding" is a way to extend battery run-time when utility power has failed by turning off non-essential devices that are drawing power from the UPS.

PowerAlert supports load shedding for any UPS that supports control of individual receptacles (plugs). The following Tripp Lite UPSs support control of one or more receptacles:

  • SmartPro 1400 (1 controllable receptacle)*

  • SmartPro 2200 (2 controllable receptacles)*

  • SmartPro 3000 (3 controllable receptacles)*

  • SmartOnline 1000RT2U (2 controllable receptacle banks)

  • SmartOnline 2200RT2U (2 controllable receptacle banks)


* This includes the RM and XL versions of these SmartPro models.

 

 

Question:
How can I see how much UPS battery run-time is remaining?

Answer:
Because of the many factors involved in the calculation of battery run-time (battery charge, load, temperature, battery discharge history, etc.), run-time values may be inaccurate, so we have chosen not to provide this value. PowerAlert does calculate output load percentage and battery capacity.

 

 

Question:
What is "Tap State"?

Answer:
Tripp Lite UPSs provide utility line conditioning to ensure a proper voltage level. If the input voltage is lower than normal, the voltage will be boosted. If the input voltage is higher than normal, the voltage will be reduced. The "Tap State" is an indication of what type of line conditioning is being used (Normal, Boost, or Reducing).

 
Documentation
Product Literature
V.12 Read Me File
V.12 User's Guide
V.12 Quick Start Guide
Resources
V.12 Installation Guide
V.12 Help Files
Related Pages
PowerAlert FAQ
Archived Software

 

     
     
     
     
 
© 2008 Tripp Lite. All Rights Reserved.